2022-11-14 10:49 PM
Hello,
When I try to build source codes including STemWin(5.40) library, following warning is shown and display is not work. when I tested at IAR 7.80.4, there was no problem.
Warning[Lt009]: Inconsistent wchar_t size
GUIAA_Char4Ext_XBF.o(STemWin540_CM4_IAR.a) and 166 other objects in STemWin540_CM4_IAR.a have wchar_t size 16 bits
__proc.o and 310 other objects, some of them in dl7M_tlf.a and 99 other libraries have wchar_t size 32 bits
When I searched iar warning info, I found this
In EWARM version 7.80 and earlier, the size of wchar_t was 2 bytes wide and the runtime attribute was set accordingly.
In EWARM version 8.11 wchar_t is 4 bytes wide and the runtime attribute is set accordingly.
As a result, we need to differentiate emWin Library by IAR version.
Could any one know where to find STemWin library to be able to support IAR 8.x?
Best Regards,
Tommy Lim
2022-11-15 4:28 AM
Hello @Tiel and welcome to the Community :)
Could you precise which package firmware are you using?
Today, STemWin-library based on version V5.44 on the STM32Cube MCU package:
/Repository/STM32Cube_FW_XX_Version/Middlewares/ST/STemWin/
You should follow the configuration steps provided in the AN4323: Getting started with STemWin Library, in section “3 How to use STemWin Library step by step�?.
Hope this helpful for you.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen