STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Graphical artifacts

Hello Forum,I’m working with a custom display that uses an ST7789V controller (GRAM) connected via FMC and MDMA.The single framebuffer is located in .RAM2.The microcontroller is an STM32H750.The application (the .text section) runs from QSPI flash, w...

Andi by Associate III
  • 930 Views
  • 9 replies
  • 1 kudos

Resolved! tnum support for fonts such as Arial

I like my digits to be monospaced so they don't dance, but I want letters to be proportional. I want to use 1 font for this. There are fonts that support this. These are called tabular fonts. They have monospaced digits and support figure space (0x20...

unsigned_char_array_0-1766157515062.png

DSI Video Mode: Shifted Image Occasionnally

I'm driving a customized LCD with STM32F469IIT6. However the image was shifted occasionnally. This issue is very hard to reproduce as it occurs 3time max a day. I'm pretty sure that the sync configs are correct. I noticed that the lane byte clock is ...

Resolved! Can't download TouchGFX version 4.26

Hello,I am unable to connect to TouchGFX version 4.26 to download or access the demo and example projects from the software download section.My system is connected to the internet; however, the application itself does not connect to the server.Please...

TouchGFX hangs on LCD::drawString()

Hello,I'm integrating the custom TouchGFX application with the SPI display on the custom hardware.Used MCU is the STM32WB55 display is based on the SSD1357, connected with the SPI.The application seem to hang during rendering of the first frame after...

pszkotak by Associate
  • 2275 Views
  • 5 replies
  • 0 kudos

Compilation error with TouchGFX application

Title modified by an ST moderator to be inline with the content. My goal is to establish CAN communication between Riverdi display - RVT50HQSFWA01 and my laptop. After developing a test GUI using TouchGFX 4.26.0, when I added the code patch for CAN c...

AnchalS by Associate
  • 314 Views
  • 3 replies
  • 2 kudos