cancel
Showing results for 
Search instead for 
Did you mean: 

pixels of various colors and not loading the gfx project

Razatana
Associate

I have a project that I've been working on for some time, but I stopped using it for a month and when I turn it on, the display only shows pixels of various colors, and I can't load the gfx onto the board. Everything was working fine before.

If I start a new project, I can load the image.

What could it be?

Razatana_0-1768165515121.jpeg

 

3 REPLIES 3
mƎALLEm
ST Employee

Hello @Razatana and welcome to the ST community,

What software are you using? TouchGFX?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Razatana
Associate

Hello,
Yes, i use TouchGFX


@Razatana wrote:

Yes, i use TouchGFX


Thread moved to TouchGFX forum board.

In that case you need to provide more information: How to write your question to maximize your chances to find a solution

- What board? 

- Project started form TBS from TouchGFX designer?

- Share your project. 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.