STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX and isomtery - isometric image

Is there any example how to create any simple animation? I would like to get object in motion using static isometric view. Object based on the few outlines of rectangles outlines with painter or putting the texture on it. I need to rotate one pseudo ...

Resolved! STM32H747XIH6 TouchGFX code generate fail!

STM32H747XIH6 touchGFX, project root directory, two seperated CM4 and CM7, touchGFX under CM7, when touchGFX designer create code, always to search .cproject under root directory, (.ioc is here, but no .cproject, only .project), under CM7 exist .cpro...

I created a button with TouchGFX, but the response to the button click is slow

Edited by a ST moderator: Please use English language in this community. Thank you ボードは、STM32F746G_DISCOを使用しています。タッチTouchGFXデザイナーにて、データ増減用のボタンを作成し、ボタンクリックでデータを増減する様なソフトウェアを構築しましたが、ボタンクリックに対して反応が遅い現象が出ています。ボタンのクリックに対して、GUI上のボタンは、反応していますが、ソフトウェア上の処理がなさ...

ベル by Associate
  • 295 Views
  • 2 replies
  • 0 kudos

Touchgfx + STM32H735G-DK Eval Kit

Hello everyone,I am currently trying to integrate TouchGFX into an existing STM32 project (an FDCAN master node application), and I am facing several issues.I enabled the TouchGFX generator in STM32CubeMX and configured all required peripherals (LTDC...

kgb by Associate III
  • 710 Views
  • 6 replies
  • 0 kudos

Resolved! Graphical artifacts

Hello Forum,I’m working with a custom display that uses an ST7789V controller (GRAM) connected via FMC and MDMA.The single framebuffer is located in .RAM2.The microcontroller is an STM32H750.The application (the .text section) runs from QSPI flash, w...

Andi by Associate III
  • 1014 Views
  • 9 replies
  • 1 kudos