STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

force update of scrollbar in scrollableContainer

I have made a dynamic menu made with a listLayout with a number of buttons inside a scrollableContainer. When a user push the buttons the listLayout is updated with new content.I have not been able to have the scrollbar reflect the size of the listLa...

mip by Associate II
  • 1974 Views
  • 19 replies
  • 0 kudos

Resolved! Incorrect Screen Output. (Shifted image)

Hello everyone.I am doing a TOUCHGFX project with STM32H750IBT6, W25Q512, IS42S32400F-6TL. I took my first screen printout and the image came out shifted. I am using my screen vertically by rotating it 90 degrees in Touchgfx Designer. I still haven't...

asdasd.jpeg
MKoca.1 by Senior
  • 2271 Views
  • 5 replies
  • 1 kudos

Resolved! Mapping external memory XSPI RAM STM32H7S7

I'm currently using an STM32H7S78-DK, and I'm correctly able to run TouchGFX with FreeRTOS and everything. I also an error handler function that, in case of a crash of TouchGFX it writes directly to the framebuffer.Now, I would like to do a similar t...

nico23 by Senior III
  • 367 Views
  • 1 replies
  • 0 kudos

Resolved! keyboard examples are the same resolution

Touchgfx 4.26.0 (and was same on 4.24.0) keyboard examples are the same resolution although there are (3) resolution of display resolution selectionsThey all display the keyboard size as approx. measured 43 mm (1.7 inches) X 33mm (1.3 inches) on a 5-...

Garbage Display

I'm very new to this so be kind.  I've been working on a display for CAN data.  I have the display designed and it works and while building code for the CAN and using the GPIO5 LED for testing, when I Run it, I get a garbaged display.  I have a worki...

IMG_1845.jpg