STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! CubeMX + TouchGFX code generation problem

Hello! First, some information. The board that I am using is a custom board with an STM32U599VJT6. It is supposed to interface an RGB666 480x480 display with parallel interface and a Sitronix ST7701S (I have correct initialization code). I am current...

Resolved! Why do I get overrun error when using DCMI?

BACKGROUNDproject purpose: capture a picture every 2 secondsboard: nucleo stm32h743zi2 at 480MHzide: stm32cubeidecamera module: ov7670 at 24MHzCONFIGURATIONThe project was initialized using stm32cubeMX with I2C and DCMI initialized. The ov7670 is con...

YL.11 by Associate II
  • 3970 Views
  • 4 replies
  • 5 kudos

Resolved! Hardfault on STM32F769 using TouchGFX

hi I use touchgfx 4.24 , STM32CubeIDE 1.16 and STM32cubeMX 6.12 I do a project with touchgfx, I import it on cubeide, no problems to launch it on the card (STM32F769I-DISCO) I make a modification ( uart 5) on the file ioc and the bilioteque (newlib r...

pascalous by Associate II
  • 5334 Views
  • 16 replies
  • 1 kudos