User Activity

How does this work with a ClickListener?I have a view with 10 custom containers. How can I tell the view when a custom container has been pressed and which one? Do you have a simple example?ThanksRegards, Roger
I have a container with a switch on my screen. On the screen there are about 20 other containers that should change their appearance depending on the switch in the first container. How can I refresh a whole screen with all elements from one container...
 We want to change the font and color of text fields at runtime. The text always remains the same. We only want to change to one of the predefined fonts.Is this possible with TouchGFX?Thank you for any advice.Regards, Roger 
Hello everyoneCan I also add an svg image to a button? I can embed images in svg format (almost) without any problems. However, if I want to assign an image to a flex button, only png works. Is there a workaround for this or does it just not work?Reg...
Does the STM32H750XBH6 have data flash memory that I can use to store 200 bytes of application data? For example to store the IP address etc.. The datasheet says something about "2 Kbytes (64 flash words) of user option bytes for user configuration"....
Kudos from