STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Template/graphics app for STM32H7A3?

Hi all,I used touchGFX before with a STM32F746-DISCO board and that worked fine to get started but now I'm looking to make a custom board with an STM32H7A3 MCU and I see nothing in the touchGFX designer for this MCU. There is an STM32H7B3 DISCO board...

Rodo by Senior
  • 2289 Views
  • 5 replies
  • 1 kudos

Resolved! STM32H7S78-DK error RGB888

Hello everyone, I present my problem.I am doing a simple project with Touch GFX on my Discovery STM32H7S78-DK. My main goal is to display images (the ones provided by touchGFX) in RGB888.I created the project and moved to CubeMX to view the .ioc file...

Resolved! General concept for non-GUI user code in TouchGFX

Hi,I´ve to start a project (with FreeRTOS) where several code has to be implemented which is not directly related to the GUI (some state machines, control algorithms, ...).I´m not sure, if I should implement this code parts as usual in my FreeRTOS an...

AWack by Senior
  • 1404 Views
  • 2 replies
  • 1 kudos

How to do a page down/up with a list

I have this ui requirement  The idea is that when the user presses the "down" button, the effect will be to go all the way down, or all the way up.  I'm using a scrollable container with a list layout to create the view, how can I do it?

JPabl1_0-1732983950201.png
JPabl.1 by Senior
  • 1613 Views
  • 2 replies
  • 2 kudos

Resolved! TOUCHGFX: is multi display possible ?

Hi,For a project I am currently working on, we have a unique custom board model on which we can flash different targets of a a same program.Depending on the target, we can work with one of two different displays, a 240x320 and a 160x80.For now, we tw...

SMarie by Senior
  • 1959 Views
  • 2 replies
  • 2 kudos

User uploading file

Hello, is it possible to allow a user to upload a file to the display? For example, if there was a usb input, the display, can read the contents or write to the usb?

Priyank by Senior
  • 945 Views
  • 1 replies
  • 1 kudos

Resolved! touchgfx simulator screen size scaling factor

hi,    Recently I notice that toucgfx simulator screen size is twice the value set in toucgfx designer, if I want the exact pixel size set in touchgfx designer while simulating, is there a scaling factor or some function to call? thanks for your time...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.