Recently, i was trying to integrate the USB-PD library from ST with the support for the STUSB1602 IC that we have on our custom hardware. I found out that the precompiled library from ST supports only the Cortex M0, M33 and M4 MCU's.... Why is that? ...
Hi,My St-link on board the STM32F7508-DK is corrupted and i cannot flash it over usb anymore.I've manage to find a Stlink V2 binary and it works ok for flashing but not for debugging.Also the V2 version does not have the ST-link in mass storage for d...
Hi,I have a STM32F779BI on a custom board that communicates with a LCD display using the LTDC interface in 16bits (480x272). I am using a single buffer inside the RAM of the MCU. So far TouchGFX works pretty well but once i activated the Software pac...
Hi, On the OpenSTLinux Git i can see that there is the warrior branch and i would like to know when will there be a realease using this branch of Openembedded?Also the Zeus branch is now available (3.0), is there plans to support it too?Thanks,
Hi there,I am trying to use the plasma-mobile enviroment as default in the x11 distro. I documented in detail everything in this issue (easy to reproduce): https://github.com/schnitzeltony/meta-qt5-extra/issues/73Can someone from ST look into this to...
@Martin KJELDSEN , I am still waiting for a solution...our product is being delayed because that feature (having an LCD + SD card working) is necessary...Thanks for answering back
Yes i have debugged the project enough to blame touchgfx for breaking the SDMMC. More than that, i have tried to set different NVIC priority for the DMA2D and LTDC needed by the TouchGFX without any impact.
I have suspected the same, it's easy to replicate, juste use a devboard with a LCD and have a TOuchGFX project active, then try to activate the SDMMC interface. I have tried it on the STM32F7508-DK and had the same issue.