STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1726 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4874 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9562 Views
  • 5 replies
  • 3 kudos

Resolved! PC15 as GPIO input on STEVAL-PTOOL4A

Hello,I am trying to use PC15 as GPIO input on the STEVAL-PTOOL4A. I configured it using CubeMX with pull-down resistor however the pin status is not changing in the software. I am sure my switch works well (checked on oscilloscope) and the LSE is di...

AnthonyK_0-1743667452123.png
AnthonyK by Associate III
  • 1035 Views
  • 2 replies
  • 0 kudos

Resolved! MC-SDK position control setting

I started working successfully with MC_SDK 6.3.2. I am doing position control application with BLDC motor. In "ST Motor Pilot v1.2.12-PositionControlApp" I want to set "Terget Position" value to values ​​bigger than the set max value. From which file...

atemur by Associate
  • 1312 Views
  • 2 replies
  • 1 kudos

Resolved! Torque command sequence

I want to confirm if the below 3 commands 1,2,3 can be given sequentially or any delay required between them. These 3 commands i am giving when a key is pressed. if(IDLE == MC_GetSTMStateMotor1()) { g_qdreference_s.q = 1000; MC_SetCurrentRefere...

STUser34 by Associate III
  • 907 Views
  • 1 replies
  • 0 kudos

DC MOTOR DRIVER

We are currently using a DCX32L motor rated at 12V and 160W, and ourmain objective is to achieve constant torque. Specifically,we need a solution that integrates current sensing with an interface that permits real-time control via software. Is this p...

spolaka by Associate
  • 825 Views
  • 1 replies
  • 0 kudos

Control 3 phase motor with STEVAL-IPM15b

Hello,​I am trying to drive a three-phase motor with the STEVAL-IPM15b, but it is not working properly. I applied 15V to Vcc and 125V or 150V to Vdc and tried testing, but the motor did not run. I checked TP5, TP12, TP6, and TP7 with an oscilloscope,...

gateSignal.png
221 by Associate
  • 911 Views
  • 1 replies
  • 0 kudos