Skip to main content
Associate
September 14, 2024
Question

STM32 and L9907 integration support

Hi,

I have a custom motor control  board with STM32F302R8T6 as controller and L9907 as the driver. Could you suggest any example codes I can use for the integration? I could not find anything available in Motor control work bench and AutoDevKit Studio.

Help much appreciated

Best Regardsm

Bala

 

This topic has been closed for replies.

3 replies

Peter BENSCH
ST Technical Moderator
September 14, 2024

Welcome @BalaB13, to the community!

I am extremely sorry, but these are two components from different application areas. L9907 is a BLDC driver for automotive applications, STM32F302 is an industrial MCU. As no STM32 has automotive certification to date, there is consequently no support for automotive devices. The same applies vice versa: Autodevkit only recognises automotive devices.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
BalaB13Author
Associate
September 21, 2024

Thanks. Could you let me know where I can get the L9907 driver files?

Peter BENSCH
ST Technical Moderator
September 21, 2024

The driver files for both automotive microcontrollers SPC560P and SPC56EL are included e.g. in SPC5-MCTK-01.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.