cancel
Showing results for 
Search instead for 
Did you mean: 

Can STEVAL-ESC001V1 Drive Low-Voltage (3-6V, 0.5A) Motors?

hashiR
Associate III

"Hello,

I am using the STEVAL-ESC001V1 motor controller and I would like to know if it can be used to drive a low-voltage motor (3-6V) with a maximum current of 0.5A. The motor is a small brushless DC motor, and I want to confirm whether this ESC is suitable for such low power requirements.

Will the controller function correctly, or are there any limitations due to the voltage and current mismatch?

Thank you!"

1 REPLY 1
Peter BENSCH
ST Employee

The STEVAL-ESC001V1 works in the voltage range 11...22V, so it cannot be used for your voltage range.

For 3...6V, 0.5A you can use the STSPIN250, for which the X-NUCLEO-IHM13A1 is available.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.