User Activity

Hello,I am experiencing an issue with my high-speed BLDC motor (47,000 RPM, 24V, 180W). Even when running the motor with no load, it is heating up more than expected, and it is drawing more current than the no-load current specified in the motor's da...
Hello all,I’m using NUCLEO F302R8 and IHM08M1 for motor control. While the motor runs, it gradually heats up to around 85°C and draws more current than its rated value in no-load conditions.while using the IHM07M1, the motor's heating seems normal, b...
Hello Community,I’m using NUCLEO F302R8 and IHM08M1 for motor control. While the motor runs, it gradually heats up to around 85°C and draws more current than its rated value in no-load conditions.while using the IHM07M1, the motor's heating seems nor...
Hi everyone,I'm trying to run my BLDC motor to its maximum torque and speed limits as specified in the datasheet. I’ve increased the supply voltage, but the motor still won’t reach these limits.Details:Using [motor/controller model, e.g., "IHM17M1 an...
 hello community, I'm using the IHM17M1 with the NUCLEO-F401RE for a low-power motor control application involving a 6V motor. The setup works well, but under load conditions (such as when the motor is underwater), the speed drops below the reference...