STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9547 Views
  • 5 replies
  • 3 kudos

FOC SDK 4.0 WebDist - no def for MCI_GetTorque

Posted on July 03, 2014 at 23:36 Hi, I just converted my project from Web Distribution 3.4 to Web Distribution 4.0 , and when compiling signed16[sMECSPEEDREF01HZ] = MCI_GetMecSpeedRef01Hz(*myMCI); signed16[sAVRGMECSPEED01HZ] = MCI_GetAv...

lumley by Associate II
  • 1241 Views
  • 2 replies
  • 0 kudos

Dual Motor control with electronic gearing

Posted on July 23, 2014 at 17:54I am using the FOC SDK 4.0 and have set up a dual motor control system with a STM32F405 controller. The motors are PMSM and have a quadrature encoder each.Now I want to drive the motors in parallel with electronic gea...

Motor control Workbench Monitor via serial

Posted on September 09, 2014 at 19:22I am trying to use the motor conrol foc library found in stsw-stm32003.  I am using an stm32f103 and am failing to understand the steps required to use the parameter files generated by the workbench so that I can...

justin2 by Associate
  • 1969 Views
  • 4 replies
  • 0 kudos

motor control in STM32 cortex M0

Posted on September 14, 2014 at 21:48Hi, would like to use STM 32 F0 for 3-phase motor control. Could anyone please let me know what evaluation board for motor control in STM32 F0 to purchase? ALso, I noticed that st’s library "STM32 PMSM FOC SDK ...

FOC 4.0 and STM32F4xx

Posted on September 18, 2014 at 21:34Hi, few days ago I downloaded the file ''STM32_FOC_SDK_4.0.0_Web_140625.exe'' from your homepage and wanted to try out the motion control on my custom board equiped with an STM32F407ZG device (either as single dr...

Problem with dspin

Posted on October 06, 2014 at 18:57 I have a computer with 64-bit windows 7 installed, when I start the dspin software it has an error message: unable to load spi_sdk.dll The application has failed to start because the side-by-side configuration...

sburr by Associate II
  • 1644 Views
  • 3 replies
  • 0 kudos

not stable at slow speeds PMSM FOC

Posted on October 30, 2014 at 15:31Hi I'm working with the motor from maxon: http://www.maxonmotor.ch/maxon/view/product/motor/ecmotor/ecmax/ecmax30/272768 When I drive the motor at slow speed (50rpm), the Speed is not stable because the resolution...

dominik by Senior
  • 1946 Views
  • 4 replies
  • 0 kudos

FOC SDK 4.2 clearing thumb mode with Eclipse AC6

Posted on January 03, 2016 at 15:27Hi,i recently ran into a problem with a FOC SDK 4.2 base motor control project.After assembling a project for Eclipse AC6 (API sources + EWARM library from web edition) I got usage faults during the execution of a ...

martin.k by Associate II
  • 1845 Views
  • 5 replies
  • 0 kudos