STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1720 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4870 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9555 Views
  • 5 replies
  • 3 kudos

FOC SDK 4.2 clearing thumb mode with Eclipse AC6

Posted on January 03, 2016 at 15:27Hi,i recently ran into a problem with a FOC SDK 4.2 base motor control project.After assembling a project for Eclipse AC6 (API sources + EWARM library from web edition) I got usage faults during the execution of a ...

martin.k by Associate II
  • 1854 Views
  • 5 replies
  • 0 kudos

PMSM FOC SDK 4.0 code stucks

Posted on March 09, 2015 at 09:32Hello,I can't get PMSM library working. I don't have motor evaluation board, i have self-built board with STM32F303RB and i have F3 discovery. Problem is that program gets lost in library instructions and ends up stu...

firmware settings questions:

Posted on March 22, 2015 at 16:32Hi!I have 2 little problem:1:My Shunt value is  0.0005 ohm. Can i set it somehow in the motor firmware.The original lowest possible value is 0.001 ohm.2:I use 1 shunt settings, and STM32F303VC controller ic. This IC ...

STM32F4DISCOVERY and STM32 PMSM FOC SDK

Posted on September 23, 2015 at 06:51Hi everyone.I am developing a robotic application and I need some advice.I need to drive two BLDC motors (these drive the wheels of the robot) and also to interface with a parallel camera.I understand that with S...

Active Braking Strategy

Posted on October 29, 2015 at 19:11I am curious how much control we have with the motor braking with SDK. We can of course dissipate extra current with a braking resistor and slow down the motor by shorting the phases. But is it possible for us to a...

STM32F405 with 2 Shunts and FOC SDK

Posted on December 02, 2015 at 14:05Hello, i want to generate a project with the WB for an existing hardware. But i can't configure the Ports for the 2 Analog Inputs of the Shunts. Can you help me to configure the project? Hardware: STM32F405 Gate D...

s61331 by Associate II
  • 1000 Views
  • 2 replies
  • 0 kudos

FOC SDK + HALL not on TIMx

Posted on January 06, 2016 at 19:54Hello, I've just designed and populated some prototyping boards which happen to connect the HALL sensor not on the correct TIM2-5 CHX pins. Instead of just throwing all in the garbage, I was wondering if is there a...

vmatos by Associate II
  • 2269 Views
  • 6 replies
  • 0 kudos