STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1724 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4872 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9557 Views
  • 5 replies
  • 3 kudos

Overvoltage error BLDC motor

Hello,I'm using the EVSPIN32G4 Eva board and MCSDK 6.2The motor is a low-induction 1pole pair 45000rpm 24Vdc Power 160WThe motor should work with a current up to 6AIn the motor profiler I cannot enter a value greater than 4A otherwise I have Overvolt...

Emanuele_0-1698770569290.png
Emanuele by Associate
  • 1776 Views
  • 1 replies
  • 0 kudos

Resolved! B-G431B-ESC1 using FOC algoritem

HiI have a smal motor (GL30) connected to a B-G431B-ESC1.I have profiled the motor and I can make a project using the 6-step algoritme.I need the motor to run in the range of 100-300rpm (almost no load), but from time to time the smooth motion are di...

Motor profiler MCSDK 6.2.0

I am moving to MCSDK 6.2.0 and want to test the motor profiler new feature. [VERSION]: MCSDK 6.2.0[TOOL]: Motor PROFILER v1.2.4EVALSTDRIVE101 + NUCLEO-F746ZG + Custom board for adapter[DETAILS]: Fail to do motor profiling[EXPECTED BEHAVIOR]:  Able to...

APerr.3 by Associate II
  • 2365 Views
  • 2 replies
  • 0 kudos

Implement brake mode and avoid overvoltage

Hi,[VERSION]: MCSDK 6.2.0[TOOL]: SDK Application Code: - single PMSM Motor- FOC- Sensorless Cordic - on STM32 G4- on the fly startup enabled- flux weakening enabled- speed controller[DETAILS]:We have a fan application with large mechanical energy and...

SF??r by Associate III
  • 3226 Views
  • 3 replies
  • 0 kudos

DRV8313 simplefoc

Hello all developers. I have a wish for you to start developing. simplefocmini (drv8313pwpr) with stm32cubeide I understand the basics of using a 3 phase timer. By creating a 120 degree difference, I can make the motor rotate but it is unstable.And I...

non by Associate III
  • 3606 Views
  • 3 replies
  • 0 kudos