STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1763 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4915 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9638 Views
  • 5 replies
  • 3 kudos

ST Motor Workbench - Placement electrical angle

Posted on March 05, 2016 at 22:10Could you describe how to set ''Placement electrical angle''. The default value in ST Motor Workbench is 300 degrees.I have an 8-pole motor with 120 degree spaced hall sensors. I have this set to 60 degrees based off...

sagpatel by Associate II
  • 6420 Views
  • 7 replies
  • 0 kudos

MC SDK start motor stucked

I'm using a STM32F4 and MC SDK 5.4.8 to control a BLDC motor from MAXON, when start the motor without load, the motor can be started everytime, but sometimes it will stucked with a load, the motor control status is still RUN, but the motor will not r...

Guopeng by Associate II
  • 1481 Views
  • 1 replies
  • 0 kudos

Why my motor jump one degree in MCSDK

Hardware : STM32G431RB + X-NUCLEO-IHM07MICurrent feedback : 3 shunt​SDK : MCSDK version 5.4.6Control mode : Position control High frequence : 25KHZMediumn frequence : 1KHZIn below image green circle can see that my motor start to move always jump one...

0693W00000LxwiXQAR.png
KLu.2 by Associate
  • 1220 Views
  • 1 replies
  • 0 kudos

Second NTC_Handle_t type sensor

uC = STSPIN32G4second sensor = PA4 (ADC2_IN17)I have tried add second NTC sensor and using MC functions.A have added:sConfig.Channel = ADC_CHANNEL_17; // BEARING_TEMPERATURE sConfig.Rank = ADC_REGULAR_RANK_1; sConfig.SamplingTime = ADC_SAMPLETIME_4...

ketchup by Associate III
  • 1789 Views
  • 1 replies
  • 0 kudos

How to run a pmsm using C-functions of mc_api.c?

I tried to run my motor (PMSM) bit it doesn't run. I used like reference the document:https://www.st.com/content/ccc/resource/technical/document/user_manual/group1/48/e6/91/f4/66/ea/48/a1/DM00490980/files/DM00490980.pdf/jcr:content/translations/en.DM...

0693W00000KZfSaQAL.png 0693W00000KZfSkQAL.png
fpaga.1 by Associate II
  • 1436 Views
  • 1 replies
  • 0 kudos

Resolved! Best method to measure temperature of STSPIN32G4

Hi,I made some temperature measures on STSPIN32G4 using a thermal camera.I saw that the central part 3x3mm of the STSPIN reaches about 70°C, while the sorrounding part does not go beyond 50°C.My question is the following: if I use the internal temper...

Resolved! Speed control

how we can change the speed of motor in STEVAL -SPIN3201 using external Potentionmeter?/or inbuilt Potentionmeter (Variable resistor )?