User Activity

I have spend some time to thoroughly understand the B-G431B-ESC1 board, which is a BLDC motor controller. According to the L6387E datasheet the high level logic threshold voltage is minimum at 3.6V. Looking at the schematic of the discovery board, th...
Hi ST CommunityI am using a default MotorControl setup with the B-G431B-ESC1 board and a BLDC motor with hall sensors. The project is generated using MC Workbench with default values. I am having a hard time to decipher the value provided by the func...
Hi ST CommunityI am working on a project where I want to use a BLDC motor for a screwdriving process. The setup is based on the B-G431B-ESC1 and a Maxon motor https://www.maxongroup.com/maxon/view/product/651618 (with a 6:1 gear added). The motor con...
Hi thereI am using a B-G431B-ESC1 board with a BLDC motor with hall sensor.The project is generated MC Workbench and is working just fine.Now I need to know the number of revolutions that the motor have taken since it was started (for application pur...
Hi ST CommunityI am having a MotorControl setup with the B-G431B-ESC1 board. The default project generated with MotorControl Workbench uses the OPAMP1, 2 and 3 and their outputs are set to pin A2, A6 and B1. These output pins are then fed to the ADC:...
Kudos from