STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32303E-EVAL

I bought the product, where can I get the basic firmware file for this product? I also want to see the basic code written in STMCUBEIDE. Thank you.

GKIM.11 by Associate
  • 1604 Views
  • 2 replies
  • 0 kudos

USB FS not sending correct amount of data

HelloI have been trying to debug an USB issue I've had on my STM32F722 Nucleo. For whatever input I try to send with CDC only two bytes are sent to my host PC. I'm using the latest HAL drivers.When breaking in the function USB_WritePacket() I can see...

Jaxc by Associate
  • 1040 Views
  • 1 replies
  • 0 kudos

STM32 USB HID keyboard with media keys

I have developed the USB HID code for keyboard. Now I wanted to add the media keys in it, like next/previous/mute/pause etc.Can I get any reference for it. Is there standard HID codes for keys or I have to change report descriptor or anything else t...

Bs.1 by Associate II
  • 936 Views
  • 0 replies
  • 0 kudos

STM32 CAN bootloader

Hello,I have a few questions regarding the system memory bootloader on STM32 cortex-M products (especially STM32F446, though other parts as well).1) Is there no timeout to get out of the bootloader if no communication is detected?I mean, the system b...

SZano by Associate III
  • 3835 Views
  • 5 replies
  • 1 kudos

To LIN communication via UART

I tried to transmit LIN communication data using HAL_LIN_SendBreak and 0x55 sync byte.The setting is 19200 bps,​ N, 8, 1​I've looked at an example using stm32Fx but it's not.​The program is in progress using TrueStudio.I would appreciate your help if...

HLee.9 by Associate
  • 1417 Views
  • 2 replies
  • 0 kudos

hard fault on start up

Hi,I'm currently experiencing a hard fault exception, when my code jumps from bootloader to application. This only happen when I reset the unit after flashing using ST link utility. e.g. If I flash the unit and does not reset, program works fine. Thi...

Cchua.1 by Associate
  • 704 Views
  • 0 replies
  • 0 kudos