STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ethernet Interfacing with STM32H743ZI2

Hello Sir,I am using the STM32H743ZI2 for the interfacing with ethernet. I am totally new to ethernet protocol. I have gone through the example lwIP_HTTP_Server_netconn and also setup all the things as per the readme.txt file .but result is not gett...

NDalv.1 by Associate II
  • 1386 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F723 USBPHYC LDO control documentation/HAL bug

So I'm looking at the reference manual of STM32F723 to find out how to control the USBPHYC peripheral. Actually there is no programmer's guide in there like for most peripherals, so I can only rely on the register map to find anything out about it. T...

Ben K by Senior III
  • 2095 Views
  • 3 replies
  • 0 kudos

SPI and IIC bus not being free and locks up. Adding/removing code or changing stack size fixes the problem.

I have seen this with the SPI bus 6 months ago. It just just happened with the IIC bus. I am using Cube 1.12.0 and this maybe related to TKube.1 issue "Potential bug in I2C HAL layer (STM32Cube_FW_F4_V1.25.0) in I2C_MemoryTransmit_TXE_BTF() ?".I ha...

RobG by Associate III
  • 2012 Views
  • 3 replies
  • 0 kudos

Resolved! Does STM32CubeMX supports SafeRTOS?

It is well known that STM32Cube IDE & MX both has quiet good support for FreeRTOS, but my question is a bit different and related to SafeRTOS, I'm just wondering if ST has support for SafeRTOS as well or not?!I'm well aware that SafeRTOS comes with l...

JJ1 by Associate II
  • 1978 Views
  • 2 replies
  • 0 kudos

How can I send data over TCP / LwIp?

I am using Echoserver and EchoClient source code for stm32. I used `tcp_echoserver_init();` function to start callback and I tried to connect with python client to this server. And its successfully connect. I checked with wireshark. And python progra...

DCtech by Associate II
  • 1191 Views
  • 1 replies
  • 0 kudos

Resolved! STM32303E-EVAL

I bought the product, where can I get the basic firmware file for this product? I also want to see the basic code written in STMCUBEIDE. Thank you.

GKIM.11 by Associate
  • 1604 Views
  • 2 replies
  • 0 kudos