User Activity

Hi there,I am using the x-cube-usb-pd in TCPM/TCPC configuration (USBPD_TCPM_LIB_PD3_CONFIG_1).My questions are:Is Augmented PDO (APDO) and variable PDO supported in this config? Or do we need to use USBPD_TCPM_LIB_PD3_FULL?If we define an APDO and w...
Hi Yohann,Created a separate thread as it's a separate issue.I am having an interesting problem with the latest USB PD library v3.I configured my board to be a source and connect to my Samsung phone (A20); it works very happily, I can start charging ...
Hello,We are using x-cube-usb-pd v3 library to implement source/sink application for our product. We've ported it to use on an STM32F030CC and using PTN5110 chip for TCPC controller. We are using configuration USBPD_TCPM_LIB_PD3_CONFIG_1.We have test...
Hi there,We have a custom board with STM32F030CC and PTN5110 chip as the TCPC. We are using the x-cube-usb-pd library with config USBPD_TCPM_LIB_PD3_CONFIG_1.Initially, DRP role is selected. When we plug in a standard USB-C charger (5V 3A output) to ...