STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! H7 USB FS default conf. using STM32Cube FW_H7 V1.8.0, not working unable to enumerate USB device

H7 Default configuration using MXCube, for USB Device FS, CDC gives error unable to enumerate USB, device not accepting address 44, error -71 and Device not responding to setup address. Board is Nucleo-H743. Using default configuration same as above,...

JBere.1 by Associate II
  • 5454 Views
  • 7 replies
  • 0 kudos

Enc424J600 with STM32L431 interface

Hello Team, I need your support to integrate the Enc424J600 ethernet IC with STM32L431, I have enabled the SPI line and trying to communicate with IC but I am not able to read the register value from the Enc424J600 chip.Ethernet State: Status led is...

How to configure the ethernet in stm32 nucleo439ZI?

I'm using the NUCLEO439ZI board.I want enable the ethernet in this board,i given all configuration in ioc, and also I'm connecting Ethernet cable my home router to board. But near Ethernet connector LED's not blinking.I'm following this example ,can ...

MVENN.1 by Associate II
  • 2159 Views
  • 1 replies
  • 0 kudos

HAL SPI Slave Receive

Dear all,I have a SPI Master, that sends out a "hello word" message working. The signals are correct and my scope can decode them.However, I can't, for the love of god get a slave working. Not DMA, not IT and not evenblocking mode.Here is my code for...

SSchu.4 by Associate II
  • 4287 Views
  • 8 replies
  • 0 kudos

Resolved! fatfs f_read() and f_gets() return incorrect data

When reading from an SD card using SPI and FAT32 using either f_read() or f_gets() the data returned does not match the actual file contents.I am using an STM32F103C8.fresult = f_open(&fil, "0:test.txt", FA_OPEN_EXISTING | FA_READ | FA_WRITE);   unsi...

0693W000006I5D0QAK.png
3nt3 by Associate
  • 3125 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F407 SPI Datasize and FSMC #WR operation DOUBLEs

Hi Team,​Basing on the lastest "STM32F4xx_StdPeriph_Driver" to Read SPI data and then write into external FSMC(8bit) device in the PWM interrupt like following .​//--------------------------------------------------------------------------------------...

0693W000006HzfNQAS.jpg
jhl14 by Associate II
  • 1418 Views
  • 2 replies
  • 0 kudos