cancel
Showing results for 
Search instead for 
Did you mean: 

Can I update the CMSIS package in STM32Cube Firmware?

A.D.
Senior

I use the current STM32Cube FW_L4 V1.15.1, but the arm_math.h is still version V1.5.3 (while there is already version 1.6 from July 2019).

Is there any way to configure CubeMX to use a different version of CMSIS then the one in the FW? I already installed CMSIS 5.6.0 under Help -> Embedded software packs - > ARM, but it seems to me like this is not used at all.

I could change the arm_math.h in the drivers path of the firmware by hand, but that does not seem to be the professional way to do this.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Piranha
Chief II

> does not seem to be the professional way

And using HAL/CubeMX non-working bloatware seems as a professional way?