STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nx_TCP_Echo_Server with static IP

Hello,I need the TCP Server with static IP address. I chose the Nx_TCP_Echo_Echo_Server example and NUCLEO-H723ZG board as a starting point. I use the STM32CubeIDE 1.19 with latest x-cube-azrtos-h7-v3-4-0 sample files. So I imported the Nx_TCP_Echo_E...

Untitled.png
Irek by Associate III
  • 1250 Views
  • 4 replies
  • 3 kudos

User Defined Context in HAL Callbacks

Hi! I have ran into an issue with the HAL that I have yet to find a decent solution to. This issue has been discussed multiple times in different contexts on the forum, and I though I would write a post to gather some of the discussions/proposed solu...

jostlowe by Associate III
  • 4642 Views
  • 12 replies
  • 11 kudos

NUCLEO-F401RE .bin file

Hello,  I'm Emily and I'm fairly new at using NUCLEO devices and ToF sensor. I would like to ask if a board NUCLEO-F401RE could only run one .bin file or could it run two .bin file? I'm currently trying out STSW-IMG035 but would like to have Gesture ...

Resolved! ADC Callback not firing with DMA

Hi all, I've recently been working on a Nucleo H723ZG with a working implementation that allows for ADC reading over DMA. I've got a Timer event that triggers it at 20kHz and it was reading and processing multiple ADCs. I've shifted to using a custom...

evanpol by Associate III
  • 782 Views
  • 5 replies
  • 0 kudos

Resolved! USBX on STM32H5 CDC - Can't open port.

Hi. Unfortunately, after several days of struggling with USBX, I'm forced to ask for your help. I'm using custom boards with the STM32h503RB and STM32h563VI. I tested the old library according to forum guides – no response when connected to a PC. The...

Jin454 by Associate III
  • 530 Views
  • 4 replies
  • 0 kudos

Low TCP/IP Data Transfer Rate Using LWIP

Edited by a ST moderator to be comliant with the ST community rules. In next time please use </> button to paste your code. Please review How to insert source code. Hi, I have a video application using F767 with LWIP and without RTOS. The custmized b...

Chao by Senior II
  • 1247 Views
  • 8 replies
  • 3 kudos