I2S Microphone Output Problems
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-03-05 7:27 PM
Hello,
I am a beginner trying to create my first STM32 project using the STM32F407G Discovery Board. I am trying to receive audio input through I2S, delay one of the channels, and then output the result to the audio jack. I can get a simple sine wave to play through the headphones, but when I try to use two SPH0645LM4H-B microphones, I only get a beeping noise through the headphones. This even happens when I don't use the delay and simply try to play the microphone input through the headphones. Sometimes making noise near the microphones has an effect on the volume of the noise. I have the microphones connected just like it says to on the datasheet and I have been trying to fix the problem for weeks with no progress. Any help or suggestions would be greatly appreciated, I am coming up on a deadline for the project and I don't know what to do. I've attached the main file and the I2C drivers to this post. Thank you for any help!
- Labels:
-
DAC
-
DMA
-
I2S
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-04-22 2:14 AM
Hi @joelnberns ,
Just some hints, not really the solution to your issue.
I would suggest you start with the source files provided in the STM32Cube package dedicated for the cs43l22 component:
That would be easy to integrate in a project you can generate from STM32CubeMX based on the required configuration you have.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.