STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can I get the CDC_Receive_FS () to read data character-by-character instead of the receiving the entire packet?

I am trying to transmit/receive data via Virtual COM port in the STM32L5xx using the USB CDC libraries. I understand that the entry to the CDC_Receive_FS() would give me an entire packet of data that I enter on the serial terminal. I would like to kn...

Jansunil by Associate II
  • 1290 Views
  • 1 replies
  • 0 kudos

Connection Problems with Nx_TCP_Echo_Client

helloWe have some problems to run the "32L496GDISCOVERY\Nx_TCP_Echo_Client" from the "STM32CubeExpansion_CELLULAR_V7.0.0" package (with AZURE RTOS).What we did so far: we changed the entries in "plf_cellular_config.h" to meet the requirements of our ...

MiEx13 by Associate II
  • 5965 Views
  • 9 replies
  • 1 kudos

STM32G431 Flash from UART Problem

Hello , I'm using Nucleo-G431RB board , and I am trying to flash the MCU via UART1 using PA9 and PA10 pins but I can't make it work .. I get an error like "Error: Activating device: KO. Please, verify the boot mode configuration and check the serial ...

BG1 by Senior
  • 5043 Views
  • 6 replies
  • 1 kudos

STM32 HID keyboard descriptor (USAGE ID codes)

Hello. I'm trying to implement a laptop keyboard on a microcontroller. I can not find usb codes for some fn buttons. The usb protocol has descriptions for combinations of changing the display brightness, volume, media keys, but more is needed. Can so...

MPano.1 by Associate
  • 2974 Views
  • 1 replies
  • 0 kudos

ST-Link Chipset

Does ST manufacturer a chip that allows integration into a project which provides USB to SWD for the additional ST32 chips? I would like to remove the need for an external programmer and just be able to add a preconfigured USB to SWD SW-Link bridge ...

JWill.10 by Associate II
  • 6223 Views
  • 8 replies
  • 0 kudos