STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H750XB USB I/Fs

Hi On STM32H750XB datasheet it says 2 x USBUSB OTG interfaces (1FS, 1HS/FS) .I configured the 1st port as FS, and the 2nd port as HS which connectd to external PHY (internal FS phy disabled) .I want to confirm that if the 2 ports can be used at diffe...

YHail.1 by Associate
  • 1108 Views
  • 1 replies
  • 0 kudos

Resolved! HAL_UART_DMAStop does not stop DMA on UART RX

Using a Nucleo-G431KB developoment board, I played a bit with UART RX DMA.I started a DMA RX on a linear buffer, and would stop and then restart the DMA.I just observed that after receiving a couple of bytes, HAL_UART_DMAStop no longer stops the DMA ...

Jack3 by Senior III
  • 7174 Views
  • 2 replies
  • 0 kudos

Can I get the CDC_Receive_FS () to read data character-by-character instead of the receiving the entire packet?

I am trying to transmit/receive data via Virtual COM port in the STM32L5xx using the USB CDC libraries. I understand that the entry to the CDC_Receive_FS() would give me an entire packet of data that I enter on the serial terminal. I would like to kn...

Jansunil by Associate II
  • 1286 Views
  • 1 replies
  • 0 kudos