STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Checking (HAL_TIMEx_MasterConfigSynchronization(&htim12, &sMasterConfig) != HAL_OK), halt the system

I am using STM32F407 with eclipse IDE. And I want to generate PWM signal using TIMER12. After all the configuration, when I call, "sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (...

Abid by Associate II
  • 3550 Views
  • 3 replies
  • 0 kudos

STM32H747I-DISCO trouble recording audio

I'm working on an audio-processing application with the STM32H747I-DISCO board (MB1166-A9). While trying out how the recording works on the board, I downloaded and built the latest version 1.11.0 from: https://www.st.com/en/embedded-software/stm32cub...

ivy by Associate
  • 1590 Views
  • 0 replies
  • 0 kudos

I'm trying to connect to Mosquitto Broker from an STM32 Azure RTOS environment using certificates that work from Paho MQTT clients

My program, linked with Paho SDK C library, works fine connecting to a UNIX-hosted Mosquitto MQTT Broker. The required SSL/TLS connection involved self-signed certificate generation. Those same client certificate sets work with "MQTT Explorer" and MQ...

AShap.3 by Associate III
  • 4006 Views
  • 2 replies
  • 0 kudos

Editing a .bin file to increase max speed of BLDC

I hope I have put this in the right forum. Will move it if not!I have a finished product so all peripherals are already selected and configured. I need to increase the max motor speed by 10%.It is a STM32F0 with single FOC and a matched BLDC.I don't ...

ANCN by Associate
  • 1869 Views
  • 2 replies
  • 0 kudos

Resolved! DRP1M1_DRP example on G0B1RE

Hello,I am trying to evaluate the DRP USB C solution ST has to offer.I have available to me a NUCLEO-G0B1RE and an X-NUCLEO-DRP1M1.I understand that the code written in the DRP1M1_DRP example was written for the NUCLEO-G071RB, but I cannot find any r...

NMartin_0-1697664479076.png
NMartin by Associate III
  • 3429 Views
  • 4 replies
  • 5 kudos

STM32F411RE bootloader via uart

Hi, I have an STM32F411RE master device connected to a slave STM32F411RE device via a UART connection. I need to update the firmware of the slave device using a UART bootloader. How can I initiate the bootloader mode on the slave device, and what pro...

Mabou.1 by Associate II
  • 1602 Views
  • 1 replies
  • 0 kudos