STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-Cube-Cellular low power

Hello all,I am working with the LBAD0ZZ1SE module, also used on the B-L462E-CELL1.I successfully adapted the "Nx_TCP_Echo_Client" Sample from X-Cube_cellular 7.1.0 to fit my needs but right now am stuck at the final step, which is the low power mode....

NHuhs_0-1698384186433.png NHuhs_0-1698384679556.png
NHuhs by Associate
  • 1120 Views
  • 0 replies
  • 0 kudos

Multiple ADC Channels (using registers)

Hello all, I am currently working on a project in which I need to sample 5 ADC channels every 50 ms. As of now, I am trying to use TIM2's TRGO (interrupt triggered every 50 ms) to trigger the conversion of a regular sequence of 5 ADC channels (PA0 - ...

caden013 by Associate II
  • 2275 Views
  • 2 replies
  • 0 kudos

P-NUCLEO-LRWAN2

I have the P-NUCLEO-LRWAN2 package. The Gateway (NUCLEO-F746ZG with the RisingHF ARDUINO® expansion board (LRWAN_GS_HF1) has a firmware VERSION: 2.1.7, Nov 6 2018. I was wondering if there is an update to the firmware and what the current version of ...

Grey by Associate
  • 1668 Views
  • 1 replies
  • 1 kudos