STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DRP1M1_DRP example on G0B1RE

Hello,I am trying to evaluate the DRP USB C solution ST has to offer.I have available to me a NUCLEO-G0B1RE and an X-NUCLEO-DRP1M1.I understand that the code written in the DRP1M1_DRP example was written for the NUCLEO-G071RB, but I cannot find any r...

NMartin_0-1697664479076.png
NMartin by Associate III
  • 3457 Views
  • 4 replies
  • 5 kudos

STM32F411RE bootloader via uart

Hi, I have an STM32F411RE master device connected to a slave STM32F411RE device via a UART connection. I need to update the firmware of the slave device using a UART bootloader. How can I initiate the bootloader mode on the slave device, and what pro...

Mabou.1 by Associate II
  • 1607 Views
  • 1 replies
  • 0 kudos

web application on NUCLEO-H723ZG

Hey. I am trying to develop a web page about the NUCLEO-H723ZG, the MCU is STM32H723ZGI want to develop a product that can be connected to the network. I want to be able to connect to my product with website on the browser and use it to control the p...

TOsso.1 by Associate III
  • 2801 Views
  • 4 replies
  • 0 kudos

Safety Compliance Advice Please

Hi All,I have recently joined a new company and I currently responsible for the Firmware design on a new product that has been externally advised that it should be rated as Class C, with regards the following standards (IEC-60730 and IEC-60335). The ...