STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! UART DMA multiple transmissions/receptions failure

Hi all,I'm facing an issue that has already been discussed several times in this and others forum, I attempted all the proposed solutions I could find but without success.I want to read the characters user inputs via Tera Term and store them in a buf...

Beppe101 by Associate III
  • 3092 Views
  • 5 replies
  • 4 kudos

STM32F373 SDADC stabilization never ends

I am working withe the STM32F373 SDADC on the STM32F373_EVAL board.When selecting the internal reference voltage (hsdadc1.Init.ReferenceVoltage  = SDADC_VREF_VREFINT1) ,the function HAL_SDADC_Init() will get stuck at while((hsdadc->Instance->ISR & SD...

BPutt.1 by Associate II
  • 889 Views
  • 0 replies
  • 0 kudos

USBX UAC2 playback issues

Looking for a bit of advice.I'm developing a full speed USB audio class device using USBX and ThreadX. So far, I've successfully rebuilt the provided example written for the H743 eval board on an F407 Discovery board. The device enumerates correctly ...

m_g by Associate II
  • 1793 Views
  • 2 replies
  • 0 kudos

USB_host MSC with stm32f746

Hi, after of much struggle in the programming, seeing the tutorial of controllers_tech, can create files and directories in usb memory. I had problems with these case, when insert the usb memory the flow of program enter in Application_Start but neve...

RMasi.19 by Associate II
  • 2053 Views
  • 1 replies
  • 0 kudos

Resolved! Init RTC failed - timeout error - stm32wb10cc

hi,I configure my micro to work on internal clock by cubemx - this is the clock configure://#############################################################################################################//                 Init Device:  System Clock Con...

aviel by Associate II
  • 3764 Views
  • 2 replies
  • 1 kudos

STM32 G0 FDCan In Classic Mode

I have a Nucleo G0B1RE board and I am trying to get the FDCan peripheral up and going.  There is no sample application specific to this board so I have copied the initialization from the C1 eval board files.  I am just trying to send classic frames (...

ttatakis by Associate III
  • 1395 Views
  • 0 replies
  • 0 kudos