Skip to main content
AFaya.1
Associate III
June 11, 2022
Question

osDelay failed

  • June 11, 2022
  • 2 replies
  • 1059 views

I am working with stm32h753zi board and i am tring to implement the task swithcing logic, if task 1 is running task 2 wait on while loop and while task 2 is running task1 should wait of while loop. I task 2 locked inside the osDelay().

This topic has been closed for replies.

2 replies

ST Employee
July 29, 2022

Hello,

In Task2 code there is no incrementation of user_count, so all will work for first 2000 iterations of Default Task (task1), then it will stay on 2001 and Task2 will stay in the first while loop.

Adding user_count++; after first osDelay(10) in StartTask02() function should solve the issue, but I would limit it from the top as it will count till max 16bit or 32bit number and the application will spend much more time in Task2 vs Task1.

Piranha
Principal III
August 9, 2022

Learn a proper thread synchronization - flags, events, semaphores, message queues...