STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F103RCT6TR-CAN

Hi,          I am MURALI SELVAM I need one solution for STM32F103RCT6TR. Which is CAN pins in STM32F103RCT6TR IC. Kindly tell me. Thank you.

murali by Associate III
  • 2986 Views
  • 4 replies
  • 1 kudos

Resolved! 3 SPI busses does not parallelize data access

STM32H743We have 4 SPI busses running at 12.5MHz but the SPI clocks are sequentially. SPI 1 and 2 are using DMA Channel 1 while SPI 3 and 4 are using DMA Channel 2. We would like them to run in parallel.Can they run in parallel.The code uses HAL_SPI_...

rlegault_0-1705436036380.png
rlegault by Associate II
  • 1128 Views
  • 1 replies
  • 0 kudos

configuration of stm32f407(SAI/i2s)

hello,I am using Stm32f407 with an IM69D120 mic. I have couple of questions regarding the interface and configuration of the mic.1) Is it possible to configure the audio codec with a 4 kHz sampling frequency and a 16-bit resolution?2) Which interface...

x-cube-eeprom - EE_Init() can I remove the step 8 ?

function :  EE_Status EE_Init(EE_Erase_type EraseType)at the end write 0 in flash:/*********************************************************************//* Step 8: Perform dummy write '0' to get rid of potential *//* instability of line value 0xFFFFF...

Giambar by Associate II
  • 4573 Views
  • 7 replies
  • 5 kudos