STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! B-L462E-CELL1 eSIM activation failed

Hello,After having purchased a  B-L462E-CELL1 eval kit with pre-provisioned Truphone eSIM and having followed the UM2743 eSIM activation steps, I still don't see the eSIM marked as activated on the Truphone IoT Dashboard after one day.Truphone suppor...

EAlai.1 by Associate
  • 2587 Views
  • 4 replies
  • 0 kudos

STM32G0B1 OpenBootloader using I2C Protocol

Hi ST Team,I'm using ST's openbootloader using i2c protocol. But facing following issues while implementing using stm32cubeprogrammer and ST-Link V3set:1. After reset the user application is not running2. Not able to flash new firmware after 1st time...

Pranil_0-1710147485386.png
Pranil by Associate
  • 1468 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F103C8 using SPI2

Hello,i am trying to interface 1.8 inch SPI TFT Display 128 x 160 to the STM32F103C8 using SPI2.https://www.az-delivery.de/products/1-8-zoll-spi-tft-displaySPI1 is used for LoRa, i thought to connect TFT too to SPI1 using addresses but i am affraid t...

hamo by Senior
  • 25235 Views
  • 65 replies
  • 4 kudos

Resolved! 1 MCU(stm32f103) - 2 Master SPI Communication error

  Hello, I am trying to control two Motor Drivers (TMC5041) through SPI communication using STM32F103. The compiler uses IAR. I am trying to communicate with two SPI Masters, but perhaps due to an initial configuration issue, only one SPI is control...

image.png
Jdogk by Associate III
  • 3868 Views
  • 3 replies
  • 3 kudos

Resolved! My own L452 board stops working when I press NRESET, problem with debbuging but not flshing.

Hello to everyone,I have crereated my own STM32L452 board with battery power supply.It dosent run as expected. Sometimes I need to discharge caps and sometimes this is not helping. When it works and I connect nreset to groung and release it stops wor...

Screenshot 2024-03-18 001022.png
HHako.1 by Associate III
  • 3083 Views
  • 4 replies
  • 0 kudos

Resolved! Turn off all GPIO pins for power

Sleep testing, How do I configure my GPIO pins to absolutely be surenone of them are supplying any power ?I wish to turn the all "off".And if there is a quick way to do it via  CubeMx , so I won't miss any ?   Thanks 

DS.4 by Senior II
  • 1381 Views
  • 1 replies
  • 2 kudos