STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L0 LPUART reboot

Hi,MCU : STM32L010R8TX.I have configured 2 UART peripheral in STM32. LPUART1 for GNSS and UART2 for LTE Module Communication. Both are working on Interrupt Mode for receiving data.Uart 2 communication is request and response based. When the LTE Modul...

nikhivv07 by Associate II
  • 1853 Views
  • 3 replies
  • 0 kudos

STM32H7 and DP83848

I've developed a custom board featuring an STM32H723GTX MCU, which is interfaced with a DP83848 PHY via an MII connection.   Additionally, I'm working with a Nucleo-F767ZI board. When configuring LWIP in the "Platform Settings", I encounter two PH...

FWupgrade_Standalone example not working

 Hi, I tried to run the FWupgrade_Standalone example on the STM32h743I EVAL Rev B board, but it didn't work.There are currently three issues 1.HS, FS in the build settings are not working correctly.If I don't connect a USB stick to the OTG HS without...

Croaker by Associate II
  • 1171 Views
  • 1 replies
  • 0 kudos

M95M04-DR - Always reading 0

I'm trying to interface M95M04-DR with XMC4700. When I read RDSR, I receive all 0s.When I write to an address, again I get all 0s on that address. I'm attaching SPI configuration and code snippet please look help me to solve this issue.I've connected...

GSaw by Associate II
  • 1627 Views
  • 0 replies
  • 0 kudos

Resolved! Can't change FreeRTOS Queue item size

Stm32CubeIDE 1.14.0, STM32CubeMX 6.10.0, STM32CubeFW_U5 V1.4.0, X-CUBE-FREERTOS.1.1.0   This started with the Stm32CubeIDE 1.14.0 release and worked fine in 1.13.x.  It happens for new projects and migrated projects.  I'm using it with an STM32U5. Go...

boxtor by Associate II
  • 3143 Views
  • 4 replies
  • 0 kudos

Multi-device communication of CAN

Is anyone familiar with CAN Communications? Hundreds of devices can communicate in the car, but I have seven or eight motherboards here, and there are always some boards that can't send data, why is this? Is there a big guy who understands?

Resolved! Couldn't make ULPI work with STM32F446.

Dear Experts,I am using a USB3300 chip as an external HS 480Mbit/s USB PHY  with STM32F446 MCU. Using CubeMX to generate code and add USB CDC Middleware. As I connect the USB Cable from the PC to the USB3300 chip no COM port is detected. Didn't find ...

YashJ by Associate III
  • 4641 Views
  • 8 replies
  • 0 kudos