cancel
Showing results for 
Search instead for 
Did you mean: 

USB Type C for charging and Power on first priority.

PVaaz.1
Associate III

Hello ,

Is it possible to use USB Type C for charging and Power as First Priority when the Wireless Charging and battery is active respectively?

Or a hardware switch or firmware is needed for this?

Also please suggest the corresponding ST USB IC and wireless charging IC for this.

The power requirement is 3A@5V (max).

Regards,

P

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nicolas P.
ST Employee

Hello @PVaaz.1​ 

Not clear to me what you want to do : charge battery through wireless AND type C at the same time ?

Cannot help you on a wireless solution.

On Type C side, 5V@3A : you don't need power delivery. So this is easy : no dedicated firmware is needed. Do you still need help on that ?

Regards,

Nicolas.