STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USBC PD TCPM with FUSB307B RXSTAT alert

Hi, I've got an issue with TCPM stack running on STM32G431 with USBPDTCPM_PD3_FULL_CM4_wc32 library.The issue is related to the configuration of FUSB307B IC registers to enable SOP messages receiver at very first SOP reception. I've posted the detail...

vostrenkov_0-1714401443054.png

STM32CubeIDE FatFs R0.12c

The FatFs version "R0.12c" provided by STM32CubeIDE is too old and buggy.I would like to ask if there are any plans to upgrade to FatFs latest version in STM32CubeIDE. As I know, FatFs used by STM32CubeIDE is open source from the site below,and the l...

hardrock by Associate III
  • 1735 Views
  • 1 replies
  • 2 kudos

FreeRTOS_MPU

STM32Cube_FW_L4_V1.18.0\Projects\NUCLEO-L476RG\Applications\FreeRTOS\FreeRTOS_MPUI am trying to debug the usage of FreeRTOS_MPU using the NUCLEO-L476RG board.But the code failed at HAL_Init() - if (HAL_InitTick(TICK_INT_PRIORITY) != HAL_OK){status = ...

HAL Functions

Diference between the below 2 funtions:HAL_StatusTypeDef HAL_I2C_Master_Transmit(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint8_t* pData,uint16_t Size, uint32_t Timeout);HAL_StatusTypeDef HAL_I2C_Master_Seq_Transmit_IT(I2C_HandleTypeDef *hi2c, u...

Resolved! Test device network speed

Hi guys,I want to know whether the device meets the 100Mbps full duplex need how to test?My own test is as follows:The device ip is 192.168.1.10, pc ip is 192.168.1.135.(The ip of pc is different in wireshark(135) and test software(25), because it is...

PeterMu by Associate II
  • 6033 Views
  • 5 replies
  • 4 kudos

Resolved! USART1 Byte length off for some reason

Hi, I am unable to interface with a sensor over RS485. I have a uart->RS485 converter hooked up to pins for USART1 (Tx on PD8, Rx on PD9) on a Nucleo-F439ZI.I also have a USBtoRS485 converter with which i'm able to communicate to the sensor fine. I h...

debug by Associate III
  • 1708 Views
  • 2 replies
  • 1 kudos