cancel
Showing results for 
Search instead for 
Did you mean: 

Windows doesn't recognise my Nucleo as a sound device

BLász.1
Associate

Hi everyone!

Sorry if it's a newbie question, I just started learning this. I used USB_DEVICE middleware to make the code for the Audio Device Class. Even though I increased the heap to 2800h Windows doesn't recognise it as a sound device. I'm using the Nucleo F446RE. Am I missing drivers? Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
KDJEM.1
ST Employee

Hello @Bálint László​ and welcome to the Community :) ,

Which Windows system are you using?

If you use Windows® operating systems: 98SE, 2000, XP, Vista®, 7, and 8.x, it should installed the STM32 Virtual COM Port Driver must be installed in this case.

Windows 10 does not require the installation of the Virtual COM Port driver anymore, as it is already built in. So, no driver is required for W10.

Also, try to use static allocation, as recommended in this FAQ.

I hope this help you!

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

The autor is talking about audio device, not CDC (virtual COM port). Next time try actually reading the topic...