STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 and DP83848

I've developed a custom board featuring an STM32H723GTX MCU, which is interfaced with a DP83848 PHY via an MII connection.   Additionally, I'm working with a Nucleo-F767ZI board. When configuring LWIP in the "Platform Settings", I encounter two PH...

FWupgrade_Standalone example not working

 Hi, I tried to run the FWupgrade_Standalone example on the STM32h743I EVAL Rev B board, but it didn't work.There are currently three issues 1.HS, FS in the build settings are not working correctly.If I don't connect a USB stick to the OTG HS without...

Croaker by Associate II
  • 1168 Views
  • 1 replies
  • 0 kudos

M95M04-DR - Always reading 0

I'm trying to interface M95M04-DR with XMC4700. When I read RDSR, I receive all 0s.When I write to an address, again I get all 0s on that address. I'm attaching SPI configuration and code snippet please look help me to solve this issue.I've connected...

GSaw by Associate II
  • 1622 Views
  • 0 replies
  • 0 kudos

Resolved! Can't change FreeRTOS Queue item size

Stm32CubeIDE 1.14.0, STM32CubeMX 6.10.0, STM32CubeFW_U5 V1.4.0, X-CUBE-FREERTOS.1.1.0   This started with the Stm32CubeIDE 1.14.0 release and worked fine in 1.13.x.  It happens for new projects and migrated projects.  I'm using it with an STM32U5. Go...

boxtor by Associate II
  • 3140 Views
  • 4 replies
  • 0 kudos

Multi-device communication of CAN

Is anyone familiar with CAN Communications? Hundreds of devices can communicate in the car, but I have seven or eight motherboards here, and there are always some boards that can't send data, why is this? Is there a big guy who understands?

Resolved! Couldn't make ULPI work with STM32F446.

Dear Experts,I am using a USB3300 chip as an external HS 480Mbit/s USB PHY  with STM32F446 MCU. Using CubeMX to generate code and add USB CDC Middleware. As I connect the USB Cable from the PC to the USB3300 chip no COM port is detected. Didn't find ...

YashJ by Associate III
  • 4633 Views
  • 8 replies
  • 0 kudos

Need Latest version for ST Link Nucleo

Kindly provide me the latest Firmware version for the above-mentioned Product along with the necessary instruction to upload it using STM32 ST Link Utility.We are currently getting old firmware issues screenshot attachedPlease assist us regarding thi...

bh0pu by Associate II
  • 4199 Views
  • 7 replies
  • 1 kudos

J2534

Anyone have J2534 support library for STM32f4 devices...?J2534 is an interface standard designed by SAE (Society of Automotive Engineers) and mandated by the US EPA (Environmental Protection Agency) for vehicle ECU reprogramming.

Vdoij.1 by Associate II
  • 1708 Views
  • 2 replies
  • 0 kudos

USB_HOST stack issue in Free RTOS

I'm using two STM32F407VGTX EVK boards to configure as host and device in BareMetal, which is working fine.I have configured (Host and Device) the same in FreeRTOS, but it is hitting hardfault error from "static void USBH_Process_OS(void *argument)" ...

usha_0-1713770415564.png usha_1-1713770442784.png usha_2-1713770472480.png usha_3-1713770498646.png
usha by Associate
  • 1108 Views
  • 1 replies
  • 0 kudos