Skip to main content
root437
Associate II
June 5, 2023
Question

ethernet interrupt not working

  • June 5, 2023
  • 11 replies
  • 5694 views

I send an ethernet packet to MAC address 00:80:E1:00:00:00 but no interrupt occurs in STM

Enabled Ethernet interrupts in CubeMX.

What could be wrong?

Code:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2023 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "string.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
 
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
 
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
#if defined ( __ICCARM__ ) /*!< IAR Compiler */
#pragma location=0x30000000
ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT]; /* Ethernet Rx DMA Descriptors */
#pragma location=0x30000200
ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT]; /* Ethernet Tx DMA Descriptors */
 
#elif defined ( __CC_ARM ) /* MDK ARM Compiler */
 
__attribute__((at(0x30000000))) ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT]; /* Ethernet Rx DMA Descriptors */
__attribute__((at(0x30000200))) ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT]; /* Ethernet Tx DMA Descriptors */
 
#elif defined ( __GNUC__ ) /* GNU Compiler */
ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT] __attribute__((section(".RxDecripSection"))); /* Ethernet Rx DMA Descriptors */
ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT] __attribute__((section(".TxDecripSection"))); /* Ethernet Tx DMA Descriptors */
 
#endif
 
ETH_TxPacketConfig TxConfig;
 
ETH_HandleTypeDef heth;
 
/* USER CODE BEGIN PV */
 
int flag = 0;
ETH_MACFilterConfigTypeDef 	macfilter;
uint8_t 		 rxBuffer[152028] = {0};
 
unsigned char txbuf[256+14];
ETH_TxDescListTypeDef * txdesc;
 
unsigned char rxbuf[256+14] ={0};
ETH_DMADescTypeDef rxdesc;
 
 
 ETH_BufferTypeDef txBuffer;
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MPU_Config(void);
static void MX_GPIO_Init(void);
static void MX_ETH_Init(void);
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MPU Configuration--------------------------------------------------------*/
 MPU_Config();
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_ETH_Init();
 /* USER CODE BEGIN 2 */
 
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 
	 if (flag == 1)
	 		 {
	 		 flag = 0;
	 		 }
	 	 HAL_Delay(1000);
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Supply configuration update enable
 */
 HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
 
 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
 
 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
 
 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
}
 
/**
 * @brief ETH Initialization Function
 * @param None
 * @retval None
 */
static void MX_ETH_Init(void)
{
 
 /* USER CODE BEGIN ETH_Init 0 */
 
 /* USER CODE END ETH_Init 0 */
 
 static uint8_t MACAddr[6];
 
 /* USER CODE BEGIN ETH_Init 1 */
 
 /* USER CODE END ETH_Init 1 */
 heth.Instance = ETH;
 MACAddr[0] = 0x00;
 MACAddr[1] = 0x80;
 MACAddr[2] = 0xE1;
 MACAddr[3] = 0x00;
 MACAddr[4] = 0x00;
 MACAddr[5] = 0x00;
 heth.Init.MACAddr = &MACAddr[0];
 heth.Init.MediaInterface = HAL_ETH_RMII_MODE;
 heth.Init.TxDesc = DMATxDscrTab;
 heth.Init.RxDesc = DMARxDscrTab;
 heth.Init.RxBuffLen = 1524;
 
 /* USER CODE BEGIN MACADDRESS */
 
 /* USER CODE END MACADDRESS */
 
 if (HAL_ETH_Init(&heth) != HAL_OK)
 {
 Error_Handler();
 }
 
 memset(&TxConfig, 0 , sizeof(ETH_TxPacketConfig));
 TxConfig.Attributes = ETH_TX_PACKETS_FEATURES_CSUM | ETH_TX_PACKETS_FEATURES_CRCPAD;
 TxConfig.ChecksumCtrl = ETH_CHECKSUM_IPHDR_PAYLOAD_INSERT_PHDR_CALC;
 TxConfig.CRCPadCtrl = ETH_CRC_PAD_INSERT;
 /* USER CODE BEGIN ETH_Init 2 */
 
 	HAL_ETH_MspInit(&heth);
 HAL_ETH_Start_IT(&heth);
 HAL_ETH_IRQHandler(&heth);
 
 
 /* USER CODE END ETH_Init 2 */
 
}
 
/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOG_CLK_ENABLE();
 
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
 
/* USER CODE BEGIN 4 */
void HAL_ETH_RxCpltCallback(ETH_HandleTypeDef *heth)
{
 
	flag = 1;
}
/* USER CODE END 4 */
 
/* MPU Configuration */
 
void MPU_Config(void)
{
 MPU_Region_InitTypeDef MPU_InitStruct = {0};
 
 /* Disables the MPU */
 HAL_MPU_Disable();
 
 /** Initializes and configures the Region and the memory to be protected
 */
 MPU_InitStruct.Enable = MPU_REGION_ENABLE;
 MPU_InitStruct.Number = MPU_REGION_NUMBER0;
 MPU_InitStruct.BaseAddress = 0x0;
 MPU_InitStruct.Size = MPU_REGION_SIZE_4GB;
 MPU_InitStruct.SubRegionDisable = 0x87;
 MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
 MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
 MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
 MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
 MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
 MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
 
 HAL_MPU_ConfigRegion(&MPU_InitStruct);
 /* Enables the MPU */
 HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
 
}
 
/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
 
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

This topic has been closed for replies.

11 replies

Pavel A.
June 5, 2023

Why is HAL_ETH_MspInit called in line 243 after Init in line 232?

Why is HAL_ETH_IRQHandler called in line 245?

Have you tried to deal with any interrupt before?

root437
root437Author
Associate II
June 5, 2023

I tried to do the order of function calls as in the documentation for the driver.

Removed HAL_UART_IRQHandler. I experimented

/*
The ETH HAL driver can be used as follows:
 
 (#)Declare a ETH_HandleTypeDef handle structure, for example:
 ETH_HandleTypeDef heth;
 
 (#)Fill parameters of Init structure in heth handle
 
 (#)Call HAL_ETH_Init() API to initialize the Ethernet peripheral (MAC, DMA, ...)
 
 (#)Initialize the ETH low level resources through the HAL_ETH_MspInit() API:
 (##) Enable the Ethernet interface clock using
 (+++) __HAL_RCC_ETH1MAC_CLK_ENABLE()
 (+++) __HAL_RCC_ETH1TX_CLK_ENABLE()
 (+++) __HAL_RCC_ETH1RX_CLK_ENABLE()
 
 (##) Initialize the related GPIO clocks
 (##) Configure Ethernet pinout
 (##) Configure Ethernet NVIC interrupt (in Interrupt mode)
 
 (#) Ethernet data reception is asynchronous, so call the following API
 to start the listening mode:
 (##) HAL_ETH_Start():
 This API starts the MAC and DMA transmission and reception process,
 without enabling end of transfer interrupts, in this mode user
 has to poll for data reception by calling HAL_ETH_ReadData()
 (##) HAL_ETH_Start_IT():
 This API starts the MAC and DMA transmission and reception process,
 end of transfer interrupts are enabled in this mode,
 HAL_ETH_RxCpltCallback() will be executed when an Ethernet packet is received
 
 (#) When data is received user can call the following API to get received data:
 (##) HAL_ETH_ReadData(): Read a received packet
*/

Pavel A.
June 6, 2023

> Removed HAL_UART_IRQHandler.

But is there an ETH interrupt handler in your code and does it call HAL_UART_IRQHandler ?

And where do you call send?

MHens.2
Associate II
June 5, 2023

Side note: Are you sure about the MAC address? all 00-00-00 after the OUI seems unlikely.

root437
root437Author
Associate II
June 5, 2023

This is the default configuration.

Ethernet transfer with this MAC is successful

Pavel A.
June 6, 2023

> DMACSR signals 0x00004080 (receive buffer unavailable) 

Where the buffers and descriptors are set up?

Please take an existing working example first and learn how it works.

root437
root437Author
Associate II
June 7, 2023

I use H743. I didn't configure DMA myself. As I understand it, the Ethernet MAC has its own DMA and it is configured in the functions: HAL_ETH_Init, HAL_ETH_Start_IT

Should I have taken any additional steps?

Where can I see a suitable example? (with up-to-date drivers and without LWIP)

Pavel A.
June 7, 2023

> As I understand it, the Ethernet MAC has its own DMA

Correct.

>Should I have taken any additional steps?

Your code does not show (or I don't see it?) assignment of DMA descriptors and memory buffers.

Unfortunately ST does not provide examples without LwIP or AzureRTOS.

Such examples IIRC were available before the "rework" (version 1.9.*)