STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C ACK Question

Hi, I bought the Nucleo-411RE board a few days ago, and try to test i2c protocol.In this MCU's reference manual(RM0383) page 492,493, about I2C register CR1, Bit 10 ACK, It explains me that acknowledge returned after a byte is received(matched addres...

giwonKIM by Associate III
  • 656 Views
  • 2 replies
  • 2 kudos

Resolved! PA0_C/PA1_C/PC2_C/PC3_C[STM32H743XGH6]

PA0_C/PA1_C/PC2_C/PC3_CWhat is the base address for the above four GPIOs that can be set?Also, do you have the following understanding about the above 4 pins?Pxy_C can be set to a pin of the same function or another function by controlling an analog ...

NiM by Associate III
  • 1082 Views
  • 2 replies
  • 1 kudos