Hello,I am having a problem with the Azure USBX MSC libraries. The version I am using is ### V6.2.0 (23-12-2022) ###. The microcontroller is STM32U545.If I connect the device to a computer with windows 7, the msc memory is mounted correctly and I can...
Hello,I need to implement AES-CBC 192 bits on micro STM32U5 serie, but hardware only supports 128 or 256 bits If i use XCUBE-SAFEA1, ST_Cryptolib is not available for U5 serie.How can i fix this issue?
Hello,I'm working on extrem low power radio with S2-LP transceiver. To obtain a very low consumption in rx mode i puted it in sniff mode. My design has external TCXO reference and when i left it always on all work fine, but if i set gpio to switch of...
Hi, Windows 11 storage driver is set by default in QUICK REMOVAL. In this mode usbx doesn't work. If i set policy in BETTER PERFORMANCE, usbx work fine. Can you help me how to setting automatically this policy? Do i need a driver or something?Thanks ...
HiI’m using the USBX libraries without standalone and without FileX. Are there any known issue with the configuration without standalone?I replicated the same issue with the NUCLEO-U545RE-Q using RAM instead of SDcard. With Windows 10 work fine With ...