STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H745I-DISCO factory reset

I purchased a STM32H745I-DISCO. The board appears to work fine. I am trying to flash the stock firmware onto the board. I downloaded the binary from the ST product page, followed the instructions, set the correct option bytes, used the external loade...

mf123 by Associate
  • 142 Views
  • 1 replies
  • 0 kudos

Resolved! UART does not work with STM32U575

Hi ST community,I create a simple application using USART1 baudrate 9600 TX pin - PB6 & Rx pin - PB7. I send uart frame each 1 second. J22 connects to CP210x. I see that the RX led of CP210x toggle each 1 second but when I open terminal screen on the...

BLS_Karo_0-1777869807138.png
BLS_Karo by Associate II
  • 290 Views
  • 5 replies
  • 1 kudos

Resolved! Boot Mode Error in Cube Programmer.

I am working with the STM32L4S5VIT6 and currently facing an issue while trying to communicate with the system bootloader over USART. I am using the B-L4S5I-IOT01A Discovery board, on which I am attempting this setup. I have configured BOOT0 correctly...

av4103 by Associate
  • 127 Views
  • 1 replies
  • 1 kudos

Resolved! ST-Link Firmware Will Not Upgrade

Hello,I've been struggling with this issue for a couple days, I have a Nucleo-L476RG board that I am trying to run and debug in VS Code. I'm using the STM32CubeMX + STM32 VS Code Extension tool chain to create cmake files, build, and then debug, but ...

sloops by Associate II
  • 2167 Views
  • 7 replies
  • 0 kudos

STLINK-V3PWR to Nucleo board SWD

Hi,I am trying to link up a Nucleo-F411RE board to a STLINK-V3PWR unit via the SWD (CN6) header.I am going to make a breakout board for the connector. See image below, I am assuming that I do not have to connect T_VCP_RX and T_VCP_TX to anything on t...

Breakout_board_connection_diagram.png