Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi everyone,I'm facing a really frustrating issue where my STM32CubeIDE can no longer detect my ST-LINK, and I've narrowed the problem down specifically to stlinkserver.exe failing to launch. This problem appeared completely randomly on my PC.Here ar...
Hello everyone i am currently working on a project with a NUCLEO-C092RC Board. With this Board i want to send OBD-II Frames to my car and receive reponses with data. I also use a LCD Display via SPI. But now i have a problem. i connected CANH/L wit...
Dear Team, We are planning to design a custom board based on STM32H745IIT6.We would like to request whether STMicroelectronics can provide any official reference design (schematic, PCB files, or recommended evaluation board) specifically for STM...
Dear STM32 MC Support Team, I recently purchased the B-L475E-IOT01A IoT development board for my project. I am currently trying to interface it with a BME668 environmental sensor and an AS7265x Spectral Triad sensor. However, I am facing an issue wh...
Hi all,I designed a custom STM32 board that powers up, but the firmware starts only after I manually press the reset button. Once reset is pressed, everything works normally. The clock source is an external crystal, and BOOT pins are configured with ...
Hey everyone, I'm having a weird issue with my STM32F4DISCOVERY board (MB997). It was working fine before, but now I can't program it anymore. Board info: Board: STM32F4DISCOVERY Device: STM32F407VGT6 ST-LINK FW: V2J46M33 ST-L...
* https://www.st.com/en/evaluation-tools/steval-usbc2dp.html#overview For the USBC2DP board is the source code available for it. I'm trying to do something similar with a N6 chip. Page for the software* https://www.st.com/en/embedded-software/stsw-u...
It looks like I have the 32F469IDISCOVERY board that looks to be powered ok via USB connector CN13, however the board doesn't appear to have demo software preloaded. COM LED LD6 flashes red. I note on the ST website that there is the 32F469IDISCOVERY...
Hello STM32 Community, I am facing a persistent "Target no device found" error when trying to program an STM32L073CZT3 custom board using a Nucleo-L073RZ as an external ST-LINK (CN2 jumpers removed). Hardware Setup: MCU: STM32L073CZT3 (custom PCB) ...
Hello everyone.I have recently made my own STM32 board based on the STM32F405. After soldering all the components and testing all pads and connections, finding them to be wired correctly and checking that the 3.3V is being supplied to all the correct...