STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can not set "nBOOT_SEL" bit in STM32L011F4 MCU.

Hello, everybody.I am developing one small application, using STM32L011F4 MCU. As I realised from datasheet, there are two ways to boot from flash memory:1)Connect PB9-BOOT0 pin to ground;2)Set nBOOT_SEL bit and use nBOOT0 bit instead of BOOT0 pin. A...

0690X000009Z68IQAS.jpg 0690X000009Z68cQAC.jpg 0690X000009Z68rQAC.jpg
MPisk by Associate
  • 2499 Views
  • 2 replies
  • 0 kudos

technical support for PCB Design

Hi sir,        I have used STM32F746BGT6 Controller for our New Project.I have used 7 & 4.3 Inch display Ethernet, SDRAM & Flash.we need the tecnical support for PCB Design.could you please help me.Regards,         M. Maha

MMAHA by Associate
  • 1043 Views
  • 1 replies
  • 0 kudos

Resolved! How to upgrade the STLinkUpgrade app.

My version of STM32CubeIDE is Version: 1.0.2 Build: 3566_20190716-0927 (UTC)The STLinkUpgrade app is 3.2.11. It says that the last firmware version is V2J31M21. However the latest version of ST-LINK/V2-1 firmware (V2J34M25))? One can use the standalo...

JFlesher by Associate
  • 1814 Views
  • 1 replies
  • 0 kudos

Pre-sales question about STM32H750B-DK

I note that the ​STM32H750B-DK comes with an attached display. If required for evaluation / development, can a larger display be connected in its place? Something in the 8" to 10" range. Touch is not needed. If so, can you recommend any brands and/or...

DLoye by Associate
  • 942 Views
  • 1 replies
  • 0 kudos

STM32 Nucleo-64 for STM32L073 gets very warm

I got a STM32 Nucleo-64 for STM32L073 board from Farnell. A few seconds after I had connected it to my PC via USB, it got so warm that I could not touch the CPU. They then send me another one, but it has exactly the same problem. I have tried setting...

KKark by Associate II
  • 2002 Views
  • 2 replies
  • 0 kudos