STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Official STM32 Nucleo-64 schematic diagram?

Hello there,I'm looking for an official STM32 Nucleo-64 development board (probably mb1136) reference schematic diagram. So I can design my own product based on that.I found some schematic on Digikey and Arrow or my team can also do but it would be g...

jarus0 by Associate II
  • 2814 Views
  • 2 replies
  • 0 kudos

Resolved! Unable to program using ST-Link

We are using STM32L476ZGTx. Until recently I was able to program the chip using ST-Link. A few hours back programming failed due to power issue and since then I have been unable to program the controller.The device connects with ST-Link Utility every...

0690X000008iOHAQA2.png
HMahm by Associate
  • 8483 Views
  • 2 replies
  • 0 kudos

"No STM32 target found" on consumer device

I'm trying to use a ST-LINKv2 to re-program a consumer device that I know has an STM32 of some kind inside (fairly sure it's a STM32L-something). I found four headers on the board that a continuity tester has shown to be Vdd, Vcc, SCLK, and SWDIO.Con...

0693W000008yDk9QAE.jpg
Jonah by Associate II
  • 6314 Views
  • 10 replies
  • 0 kudos

Resolved! Error in initializing ST-Link device. Reason: (-1) Unknown. Please check power and cabling to target.

When I tried to debug my STM32F303RE nucleo board with Truestudio , I get this messages from console:When I get this message , I was working on EXTI interrupts at register levelSTMicroelectronics ST-LINK GDB server. Version 5.1.0 Copyright (c) 2018, ...

AAdin.1 by Associate II
  • 4528 Views
  • 1 replies
  • 1 kudos

Resolved! I got two STM32H735 Discovery kits (STM32H735G-DK) and broke them somehow by connecting both via USB at the same time. A) What causes these problems and what can be done to avoid them? B) What can be done to revive the boards?

I performed the following steps:1) Set JP7 to STLK2) Connect USB -> Demo starts correctly3) Flash a simple self-written code (sets LED to state of user-button) via OpenOCD -> ST-Link works4) Flash a second self-written code (sets both LED to state of...

KNeus.1 by Associate
  • 2359 Views
  • 3 replies
  • 1 kudos

Resolved! NJTRST (PB4) pin for stm32l431

Hello, thereI was not able to use the NJTRST (PB4) pin as a general GPIO input pin. I googled and other people having the same issue using the macro: __HAL_AFIO_REMAP_SWJ_NONJTRST()to remap the NJTRST pin. Yet, this macro is not available for the STM...

ELin.4 by Associate II
  • 8007 Views
  • 7 replies
  • 0 kudos