STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F407 First Programming Failed

Hello Community!I have a project where I was using a STM32F407 MCU from a minimal ready-to-run system with USB, programming connection and pin headers to access every MCU pin. While using this hardware, the project can be loaded and executed on the M...

ÀTorr.1 by Associate
  • 1430 Views
  • 2 replies
  • 0 kudos

Hello, I am new to STM32 and keil µvison5.I have a STM32F407VGT6 I wrote a code and it's build successfully . But when I try to load ,it says "NO ST-LINK detected "Cannot enter debug mode" and "Error:flash Download Failed-Target DLL has been canceled"

I reinstalled everything from keil to the st-link utility. I reinstalled the driver en.stsw-link009 . But still the same problem. Also it's not detected by the st-link utility.So, any solutions ?

NSOLT.1 by Associate II
  • 2526 Views
  • 6 replies
  • 1 kudos

STM32L552 SMPS hardware design

I have a question about connecting of the SMPS V15SMPS pins. From the datasheet we see, that the V15SMPS_1 and V15SMPS_2 pins are connected internaly. But, on the "Figure 6. SMPS step down converter power supply scheme" they are alco connected extern...

Schematic for STM32F469I-DISCO B03

Last week I bought a few STM32F469I-DISCO boards from DigiKey. Today I wanted to look at the schematic and found that there are two revisions available, B07 from 2015 and C01 from 2020.  But I have B03!  I'm wondering how old my board actually is, an...

Resolved! STLink Utility v4.6.0 does not run

It complains about not finding mfc140.dll.I do have mfc140.dll in C:\Windows\System32.What next?JW[EDIT] The CLI does not run either, throws the same error:  After copying mfc140.dll into the directory where the stlink-utility executable is located (...

0693W00000ALzUYQA1.png 0693W00000ALzTGQA1.png

Resolved! [NUCLEO-F722ZE] EXTI15_10_IRQ

Hi,I wanted to generate interrupt on pins PC14 and PC15 on NUCLEO-F722ZE board but it doesn't work. In the board documentation I found that jumpers configuration should be as per screenshot. Since elements there are pretty small and I don't want to d...

0693W00000AM91HQAT.png
SHutc.1 by Associate
  • 1279 Views
  • 1 replies
  • 0 kudos