Any boot flash is required for this IC, Any standard JTAG pin out and connector part numbers are available.Decoupling capacitor and crystal values are need to verify.
Hi berendi,The address collision will be taken care in the I2C bus. Pull Up resistor added for I2C resistor.We will plan to use internal oscillator.Can you please share the JTAG pinout and target board connector part number for V3SET.regards,selvakum...
Hi Piranaha, Thanks for your comments , I will update the C33 and C34. I will check the recommended application note for crystal.We planned to use V3SET Programmer. So we need Target board 20pin JTAG connector part, Can you please suggest.regards,sel...
Thanks Jack Peacock_2.Here with i attached power consumption and crystal capacitor values.i found power consumption of controller is ~35mA is the maximum current. Is it right one. Then based on application note for crystal oscillator capacitors are f...
Sorry , i missed the attachment. Need to review this schematic. in the following aspect : 1.Any boot flash is required or not for this controller. If yes provide the details.2.JTAG interface connector interface, Connector part number and matting flas...