Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
i searched in different sites (digikey , mouser...) to find the footprints and schematics that you have used but i dont find the exact ones , if you can help me it would be awesome ,i am actually working on a luxmeter prototype and am using the ST32F...
Hi community. I have bought a new st link / v2 A 2022 08. I am able to program my microcontroller with stm32cubeide as shown below but when I try to program it which the same version of stm32cubeprogrammer I am not able to do it.. I click on connec...
Hi everyone,I'm trying to program a pcb which has STM on it as MCU. Using Nucleo board Stlink but it gives error. Target no device foundError in initializing ST-LINK device.Reason: No device found on target
I am using STM32F030C8T6TR. An external 8 mhz oscillator was connected to the OSC_32_IN-OUT input by mistake, not to the OSC_IN-OUT pins on the board I have. Hardware cannot be changed. Can I reconfigure the pin with software or How can I use it? I a...
There is St-link embedded for the stm32f407 card, but I don't know how to use it, is st link v2 still required to debug it? Please help I'm going crazy.
STM32F103CBT6 is the same MPU used on the Nucleo demo boards as an ST-Link implementation.Is it possible to get these processors pre-programmed with ST-Link firmware?Under what conditions, if any?
STM offers a utility to convert an ST-LINK debugger to J-LINK debugger.USB drivers are current.But when "stlinkreflash.exe" is run [in admin mode], it says "cannot find an ST-LINK, multiple ST-LINKs are plugged in, or ST-LINK in use".None of that is ...
The STM provided USB host project has the following readme text:- STM32H7B3I-EVAL Set-up - Plug the USB key into the STM32H7B3I-EVAL board through 'USB micro A-Male to A-Female' cable to the connector: - CN8 : to use USB High speed (HS), Make sure...
what's the dimension of STM32F746IEK6. Especially for thickness, is there any tolerance ?