cancel
Showing results for 
Search instead for 
Did you mean: 

Can I program STM32 U585AII6Q with ST-LINK/V2?

ASavi.3
Associate II

I made my own PCB with STM32U585AII6Q and there are pins SWCLK, NRST, SWDIO, GND, VDD which I connected to the ST-LINK/V2. When I try to program STM32 U5, I always have error "No device found on target".

Is there a problem with ST-LINK/V2, do I need to use ST-LINK/V3?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
ASavi.3
Associate II

Thank you!

Everything is fine since I programmed STM32U5 via STM32CubeProgrammer.

View solution in original post

3 REPLIES 3
Mike_ST
ST Employee

Hello,

ST-Link V2 works with STM32U585 too.

TDK
Super User

Yes.

Is the board powered? Is a voltage detected in STM32CubeProgrammer?

If you feel a post has answered your question, please click "Accept as Solution".
ASavi.3
Associate II

Thank you!

Everything is fine since I programmed STM32U5 via STM32CubeProgrammer.